Other Parts Discussed in Thread: CC2640
Tool/software: Code Composer Studio
Hi again.
I'm trying to use mpu6050 with cc2640 launchpad.
I started i2c with tidriver example i2ctmp007 and trying editing the example a little bit.
Here's a part of code
/* Turn on user LED */
GPIO_write(Board_GPIO_LED0, Board_GPIO_LED_ON);
printf("Starting the i2ctmp007 example\n");
/* Create I2C for usage */
I2C_Params_init(&i2cParams);
i2cParams.bitRate = I2C_400kHz;
i2c = I2C_open(Board_I2C_TMP, &i2cParams);
if (i2c == NULL) {
printf("Error Initializing I2C\n");
while (1);
}
else {
printf("I2C Initialized!\n");
printf("let's go!");
}
I'm using printf to check where error occurs, and there's strange thing happening.
Console print "I2C Initialized!" but not "let's go!".
I have no idea what the problem is.
Anybody knows..?
Thank you!