Part Number: CC2650
Tool/software: Code Composer Studio
My customer got a problem in importing project into CCS, and need your guidance to solve this problem.
He has several ARM compiler in his computer, and the latest version is v17.6.0.STS. He exported the CCS project and tried to import it into CCS in another computer, whose latest compiler version is v16.9.3.LTS. A error occurs saying lack of compiler v17.6.
Then, He set the compiler to v16.9.3.LTS in his computer, and exported again. The same error occurs when he imported it in another computer with compiler v16.9.3.LTS.
it seems that if the highest version of the two computer is different, the project in the computer with higher version compiler can not be imported into the other computer. even the higher version compiler is not used but just exist.
Please guide a way to export project from CCS on a computer with higher version of compiler, and make it importable on another computer with lower version of compiler.
Or, please help to confirm the highest version of compiler MUST be the same to export/import project.
Thanks!