Part Number: F28M35H52C
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Need some help running xds 510 SD debugger on concerto cortex m3 core.
i am using a C2000 based F28M35H52C Control Card along with Docking station.
For software development till date, i used inbuild XDSv100v2 version debugger for software debugging. But now when i tried to use XDS 510 spectrum digital debugger using 10 pin JTAG connector on the docking board i am having problems.
To be more specific,
The problem i see is only when i try to debug the cortex m3 core of the controller. Meaning i can debug c28 core using xds 510, but not cortex m3 core. The error pop up message i get when i try to debug cortex m3 core is as below:
Load program Error.
Target must be connected before calling the function.
I am not sure if it has to do something with gel file. Because as i already mentioned the USB JTAG works perfectly fine for both the core.