This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with USB200 - No source available for "0x3ff9fa"

Hi everybody,

I have created one simple application (gpio output pin toggling), but if I try to debug it with USB200 emulator, this message will appear: "No source available for "0x3ff9fa". On the other side, if I decide to use on-board debugger XDS100v2, there is absolutely no problem. Why?

I have got F28335 Control card and C2000 Peripheral Explorer, the CCS is in version 6.2.0

The whole application is similar to code, which you could find in "F2833x-F2823x Firmware Development Package User´s Guide" document.

Thank you a lot.

Miroslav