This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCS in-program update broke installation...

Tool/software: Code Composer Studio

Hi,

I'm running CCS Version: 7.2.0.00013. A week or so ago, my installation tried to update as it does every so often, but it failed on multiple counts - so many, but I can't state which was the first it failed on... whilst my dev environment "seems" to be running OK, the whole update process is now broken - it fails immediately as shown below. This is a Windows 10, 64-bit, Intel Lenovo system - never has any issues and no funny drivers installed.

I have GIT installed plus MSPware, but nothing else. I'm using the FET programmer and standard Launchpads

Any ideas welcome, preferably those that don't involve scrubbing my installation and starting again! That would be grim indeed...

Thanks