This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CCSTUDIO-C2000: Debugging two devices in single board and creating Target Configuration File for simultaneous debugging

Part Number: CCSTUDIO-C2000

Tool/software: Code Composer Studio

In my custom board I have two C2000 devices one is TMS320F2810 and TMS320F28335. JTAG is connected in Daisy Chain method, i used to debug both in earlier version of CCS3.3, and and it is working. Now i migrated to CCC V5.5, so how can i do the same thing in CCS V5. so my concerns are 1. How do i create the Target configuration file? 2. How to connect each firmware/code to each device for debugging simultaneously?

thanks and regards,

Arun Gopalakrishnan