Tool/software: Code Composer Studio
Hi,
I want to use the uniflash software to download two flashs.
I use Spectrum Digital XDS510UUSB Emulation probe and 2 flashs TMS320F2812.
I have an error because my configuration file ccxml is empty.
The error is as follows : "Error connecting to the target: Error 0x80000200/-1041 Fatal Error during : OCS, Device driver: Problem with the Emulation Controller. it is recommendeds to RESET EMULATOR. this will disconnect each target from the emulator. the targets should then be power cycled or hard reset followed by an emureset and reconnecter to each target."
How to create the configuration file ccxml ?
Regards,
Denis.