This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
I am seeing an optimization issue with C2000 compiler v16.9.3.LTS. A CCSv7.2.0 test case is attached. The problem is the following function in the file test.c:
typedef struct
{
int m1;
int m2;
} SD;
const SD D[2] = {{1000,1000},{1000,1000}};
int DemonstrateOptimizationIssue()
{
int i;
unsigned long v1 = 0;
int v0 = 1, v2 = 0, v3 = 0;
for (i = 0; i < 2; i++)
{
v1 += (unsigned long)(D[i].m2) * v0;
v2 += D[i].m1;
v3 += D[i].m2;
v0 += i;
}
v1 = v1 / v3;
if (!v1 && !v2) return(0);
return(1);
The correct return value is a 1. If you invoke -o3 optimization for test.c, you get a return of 0. The compiler seems to disregard a number of the calculations, including the multiply of v1. This wouldn't concern me normally since these are local vars and the value of them is never used outside this function, except that here the return value is wrong!
The build line is:
"C:/TI/ccsv7/tools/compiler/ti-cgt-c2000_16.9.3.LTS/bin/cl2000" -v28 -ml -mt --float_support=fpu32 -O3 --include_path="C:/TI/ccsv7/tools/compiler/ti-cgt-c2000_16.9.3.LTS/include" --include_path="C:/D/dsp/work/F28335_example_nonBIOS_ram/include" --include_path="C:/D/dsp/work/F28335_example_nonBIOS_ram/DSP2833x_headers/include" --define=EXAMPLE_NONBIOS --define=EXAMPLE_RAM -g --diag_warning=225 --display_error_number --quiet -k --asm_listing --c_src_interlist --output_all_syms --preproc_with_compile --preproc_dependency="src/test.d" --obj_directory="src" "../src/test.c"
Could I get a sanity check here that this isn't an infirmity in the C code (e.g., a missing volatile that is needed or something).
Thank you,
David
Thank you for notifying us of this problem, and sending in a concise test case. I can reproduce it. I filed CODEGEN-3655 in the SDOWP system to have this addressed. You are welcome to follow it with the SDOWP link below in my signature.
Thanks and regards,
-George