Part Number: TM4C1294NCPDT
Tool/software: Code Composer Studio
Hi,
I try to use the RTOS analyzer in code composer studio (Version: 7.2.0.00013). The first time I tried to use it in the tools menu, there was a dialog telling me that it needs to initialize. After I clicked on OK, it showed a dialog box with a progress bar saying "initializing use cases" for a short moment and the dialog box disappeared and after that nothing happened and the RTOS analyzer menu option disappeared from the Tools menu. If I close code composer studio and start it again, the menu option is shown again however, the same scenario as above is repeated when I try to run RTOS analyzer. Also, the same behavior happens if I try to run system analyzer.
Is there any additional steps to do before running these tools?
Thanks for your help,
Sina