This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/MSP430FR5972: DIVIDE_MULTIPLICATION OPERATOR IN MSP430

Part Number: MSP430FR5972

Tool/software: TI C/C++ Compiler

Hi Experts,

I am using the MSP430FR5972 microcontroller for my project and IDE is Code composer studio v7.I need to calculate battery voltage  for which I need to use multiplication (*) and divide operator(/)

When I use divide operator(/) I receive this warning :

@WARNING: Detected Divide Operation(s).Recommend moving them to RAM during run time or not using as these are processing /power intensive.

I need to know the reason for this why the compiler is throwing this error and whether multiplication and divide operator is recommended to use and if not why?

Thanks In Advance.

  • Himanshu,

    I see that you have a duplicate post here that has already been responded to. To avoid duplicate work, we will go ahead and close out this thread but if you have a new compiler issue/question please feel free to start a new post. Thanks!