This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1310: Debugging CC1310 with the MSP-FET Flash Emulation Tool

Part Number: CC1310
Other Parts Discussed in Thread: MSP-FET, , TMDSEMU110-U

Tool/software: Code Composer Studio

Hi everyone,

I got a LAUNCHXL-CC1310, and I'm currently doing a project with the CC1310. I recently got as a gift the MSP-FET Flash Emulation Tool, but I'm not using any MSP-Family MCUs... so I'm trying to find if there's a way to connect the MSP-FET Flash Emulation Tool with the CC1310 in order to debug with it on the CCS v7.

I've checked that other people have tried with the MSP Launchpad or with the CC1310, but I can't seem to find anyone using the MSP-FET Flash Emulation Tool specifically on something like this. I checked out the device's datasheet, and found the following compatibility device table:

It says that it has 2-wire JTAG, and the CC1310 has a cJTAG and 2-wire JTAG, so is there a way to connect both of them to debug/program the CC1310 using the MSP-FET Flashing Emulation Tool?

Thanks, Alan.