This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv 4.1.3 - CGT declared as "not installed"

Hi Champs,

out of the blue my computer complained that it could not build a project any more. Further analysis showed that the CGT version given in the project settings was declared as "not installed". I double checked several times, finally deleted all TI software, as well as all registry entries with "Texas", but the problem remained (see attached pictures). Even if I do a 100% standard installation of CCS4 (where CGT is installed), this CGT installation is not found.

Can you please help.

Kind regards,

one and zero