This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Possible CCS v3.3 Simulator error

When using the C6747 cycle accurate simulator in CCS 3.3.82.13 I get a seemingly spurious message, "Error: Trigger word not programmed for QDMA channel 0". The simulation then proceeds to hang. Note that the code being simulated works on target without any issues. I verified that I had indeed initialized the QCHMAP0 register in the channel control register for trigger word = 7. Is this a known issue with the simulator? If so, how do I fix it?