Part Number: EVMK2H
Tool/software: Code Composer Studio
Hello,
I have just installed CCS6 on CentOS 6.6, ran the driver install script, and then attempted to test the connection with my EVMk2H on board probe. Every time it fails. I have attempted updating CCS, then uninstalling and reinstalling the pod drivers and nothing has worked yet.
Here is the output from the error window:
[Start: Texas Instruments XDS2xx USB Onboard Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
/home/user/.ti/ti/0/0/BrdDat/testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-600' (0xfffffda8).
The title is 'SC_ERR_LIB_ANY_LOCATE'.
The explanation is:
A required dynamic library could not be located.
The library isn't on the search path.
[End: Texas Instruments XDS2xx USB Onboard Debug Probe_0]