Part Number: TMS320VC549
Tool/software: Code Composer Studio
How does one read and write to IOPORTs in the debugger. When the memory window is set to IO nothing shows. Moving the cursor over the memory display window displays the error:
Address 0x0
Error: Memory map prevented reading 0x0000@IO.
If you type "PORT_READ 0" in the Scripting Console you get:
TypeError: PORT_READ is not a function, it is java.lang.Double.
So how does the beleaguered programmer read an IO port on a c549 with CCS 5.5?
Thanks, Paul