This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AM4376: How do I create a CCS project for a custom board with a AM4376 and TI-RTOS?

Part Number: AM4376


Tool/software: Code Composer Studio

How do I create a CCS project for a custom board with a AM4376 and TI-RTOS?

When a I create a CCS project and select the TI compiler, the Target do not seem correct and list of Platforms does not have AM437x. If I select the GNU (Linaro) compiler, the Target and Platform look like correct. Can I use the GNU compiler?
CCS 7.2.0.00013
ti-processor-sdk-rtos-am437x-evm-04.00.00.04.

Thanks in advance.

Marcio