Other Parts Discussed in Thread: CCSTUDIO
Dear experts,
I am newbie for CCS, i have installed CCS v3.3 and DSK 6544 packages which has come along with the kit.
When i build the LED example present as part of it, it built properly and i was able to load .out file. Then i created my_led project added all the files of LED project to it then built it, got the following error, (And again i build the LED project , got same error)
------------------------------ led.pjt - Debug ------------------------------
[led.tcf] "C:\CCStudio_v3.3\bios_5_31_02\xdctools\tconf" -b -Dconfig.importPath="C:/CCStudio_v3.3/bios_5_21/packages;C:/CCStudio_v3.3/bios_5_31_02/packages" led.tcf
Build error: cannot run cl6x.
Build error: cannot run cl6x.
Build error: cannot run cl6x.
Build Complete,
3 Errors, 0 Warnings, 0 Remarks.
What could be the problem??
Regards,
Ashwini