Part Number: TMDSEVM6657
Other Parts Discussed in Thread: TMS320C6657
Tool/software: Code Composer Studio
Hello,
I am using CCS v5 and I attempting to access the TMDSEVM6657 EVM Board. I am following the BiosMulticoreSDK_2.1_GettingStartedGuide and I am setting up a new target configuration. I have followed the guide successfully when I chose the connection as Texas Instruments XDS100v1 USB emulator and the device as TMS320C6657, but the next instruction tells me to "Select the EVM device as specified in the Target Config figure" (which I assumed was to click the Target Configuration link under the Advanced Settings) and the image of what I see is below. I don't see where the EVM device is suppose to be.
When I attempt to configure the file I receive the following results:
In the Debug window:
Texas Instruments XDS100v1 USB Emulator_0/C66xx_0 (Disconnected : Unknown)
Texas Instruments XDS100v1 USB Emulator_0/C66xx_1 (Disconnected : Unknown)
In the Console window:
Error connecting to the target:
(Error -600 @ 0x0)
A required dynamic library could not be located.
The library isn't on the search path.
(Emulation package 5.0.838.0)
Am I missing some file for the TMDSEVM6657 board or some software? Any help would be greatly appreciated.
Thank you,
Joseph