This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CCSTUDIO3: Installation issues in Windows 10

Part Number: CCSTUDIO3


Tool/software: Code Composer Studio

Hi,

I was able to install CCS3.3 SR12 on a Windows 10 machine and make it work. When i tried a different machine then the process tries to start as i can see a splash window that comes and then disappears. In task manager i can see the process and it exits as soon as splash window disappears.

I am not sure what is the difference between these 2 machines that is causing it. Both have same version of Win10 build. Both have UAC off and antivirus it turned off. Is their any log which i can look at and identify the issue?

The reason to use CCS 3.3 is that i am using MATLAB which has some functionalities supported only with CCS 3.3. Moving to a new CCS will require lot of man hours of effort and is not very practical.

Thanks.

  • Hi Rahul,
    CCSv3.3 was never officially supported on Windows 10 hence we cannot provide much support. I personally have never been able to get CCSv3.3 to work well on Windows 10. There was one forum member who was successful and shared the below tips:
    e2e.ti.com/.../2290735

    Otherwise I don't have much more insight to offer. Good luck!
    ki