Part Number: RF430FRL152H
Other Parts Discussed in Thread: MSP-FET, UNIFLASH
Tool/software: Code Composer Studio
I've successfully built an application based heavily on the sensor hub project. Can program our custom 152h-based board using CCS to build the app, then program it using a MSP-FET. We're now ready for production, which requires two variants of the application. I've saved the two *.out files for manufacturing.
My question is whether CCS can be used in a manufacturing environment, where they don't want to build the apps, but rather just load the *.out files then program the part.
I've been searching for how I can use the binaries. I can launch CCS, build my project, program the part, load the binary, program again. The result is a non-working application.
Looking for a suggestion on how to load & program the *.out binaries, either in CCS or another stand-alone application.
Thank you for reading this post!
Ken