This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6657: Install of discovered products fails

Part Number: TMS320C6657


Tool/software: Code Composer Studio

Hello

since a few days ago I get an error whenever I try to update (inside CCS Version: 7.2.0.00013, on Windows 10x64):

To get there, I went to Window->Preferences->CCS->Products and clicked on "Rediscover".

Is there a work around?

Thank you !

Kind regards,

Pablo

  • Pablo,

    Do you see that error when installing any of those discovered products? I see that the message refers to the NDK package. Could you deselect the NDK and see if the others are installed properly.? Or perhaps try selecting only one of them at a time and see if that helps?

  • Hello AartiG

    I tried the packages separately. The error appears only with NDK.

    I'm not using that package right now, so it is not a big issue. If you would like more context information, just ask (do please specify).

    Kind regards,

    Pablo

  • Pablo Stickar said:
    I tried the packages separately. The error appears only with NDK.

    There is a known issue with that specific version of NDK. Please see this post where the same issue is discussed. The first link referenced in that post describes the issue and the recommendation of installing the patch for the MCSDK (available here).