This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1310: Does CCS support Attach function similar as IAR

Part Number: CC1310

Tool/software: Code Composer Studio

Hi Team,

I would like to check if CCS support Attach function, it's useful to debug some issues.

When the device was run or hung in some places, we can connect to CC1310 device via JTAG without RESET.

Then we can use CCS attach to the device and see where is the sw running.

IAR has this function.

Thanks.

Victor Xu