Tool/software: Code Composer Studio
Hi everyone,
I'm building a program using project_zero example and when I tried to change the Board files to other ones this error start to appear:
makefile:187: recipe for target 'colmeiaV2_1_app.out' failed
"c:/ti/simplelink/ble_sdk_2_02_01_18/src/common/cc26xx/ccs/cc26xx_app.cmd", line 121: error #10099-D: program will not fit into available memory. placement with alignment fails for section ".const" size 0x22f3 . Available memory ranges:
FLASH size: 0xc000 unused: 0x1ad max hole: 0x1a2
FLASH_LAST_PAGE size: 0x1000 unused: 0xfa8 max hole: 0xfa8
error #10010: errors encountered during linking; "colmeiaV2_1_app.out" not built
gmake[1]: *** [colmeiaV2_1_app.out] Error 1
gmake: *** [all] Error 2
Then I change again the Board Files back to the first ones, I also delete it and import it again and the error persists.
The same program with the same files works fine in other PCs.
What happens? How can I use the program again? If you need more information, I will provide.
Thank you and best regards,
Miguel Vieira