Other Parts Discussed in Thread: OMAP-L138
I am currently able to connect to my OMAP-L138 (C6748 side) using a XDS510 USB Emulator without any problems. However, I was trying to get a co-worker's machine to work as well and when he tries to connect to the target using CCS4 (Premium version) it will hang. If he tries to connect to the target using CCS3.3 (again trying to connect to it as a C6748) he will get the following error. Does anyone know why I would not receive this error with my setup but he would see this issue?
Again, on my setup, it all works with exactly the same hardware.
Trouble Reading Memory Block at 0x1c10800 on Page 0 of Length 0x4: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
GEL: Error while executing OnTargetConnect(): target access failed.
Trouble Reading Memory Block at 0x1840020 on Page 0 of Length 0x4: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
Trouble Reading Memory Block at 0x1840040 on Page 0 of Length 0x4: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
Trouble Reading Memory Block at 0x1840000 on Page 0 of Length 0x4: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
Trouble Reading Memory Block at 0x184a600 on Page 0 of Length 0x40: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
Trouble Reading Memory Block at 0x184a640 on Page 0 of Length 0x40: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
Trouble Reading Memory Block at 0x184ae00 on Page 0 of Length 0x40: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
Trouble Reading Memory Block at 0x184ae40 on Page 0 of Length 0x40: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
Trouble Reading Memory Block at 0x184a200 on Page 0 of Length 0x80: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
Trouble Reading Memory Block at 0x184a280 on Page 0 of Length 0x80: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
Trouble Reading Memory Block at 0x1c00004 on Page 0 of Length 0x4: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
Trouble Reading Memory Block at 0x1c00004 on Page 0 of Length 0x4: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
Trouble Reading Memory Block at 0x1c00004 on Page 0 of Length 0x4: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
Trouble Reading Memory Block at 0x712104 on Page 0 of Length 0x340: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.
Trouble Reading Memory Block at 0x712104 on Page 0 of Length 0x300: Error 0x00000002/-1194 Error during: Memory, The memory ID is not supported by the hardware.