Hello,
Does anyone have some hints on this error received when trying to connect XDS510PP plus to DM365 using CCSv3.3.82.13? The CCS config file is from http://support.spectrumdigital.com/boards/evmdm365/revf/files/DM365-XDS510USB.ccs JTAG clock is at 10MHz. Since the error is on connect, I suspect the gel is inconsequential.
Fatal Error during: Memory, Initialization, OCS 0x80000242/-1060.
If I retry I get another error message:
Fatal Error during: OCS, Control 0x80002200/-173,
which is repeated if I retry again.
SD Config results:
** Checking emulator/eZdsp scan connection ** Emulator Test ** $$ EmuProductName=XDS510PP_PLUS $$ EmuPortAddr=0x378 $$ EmuPortMode=SPP8 \ $$ ProductId=10 $$ ProductVersion=02 ** Emulator Scan Test -- Found JTAG IR length of 6 -- Found 1 JTAG device(s) in the scan chain Also: the same emulator works fine with a non-DM365 board and the board connects fine with a 560 PCI Any hints? Thanks, Katie