Part Number: TMS320C6657
Tool/software: TI C/C++ Compiler
The customer used ccs7.1 and compiler version 8.1.3.
When build the following code:
omp_set_dynamic(1);
#pragma omp parallel for
for (k = startScale; k <= endScale; k )
{
.......
}
error:
INTERNAL ERROR: C:\ti\ti-cgt-c6000_8.1.3\bin\acpia6x.exe experienced a segmentation fault
while processing function DetectFaceVideo file ../src/LearnGAB.cpp line 902
This is caused by a defect in the compiler itself. TI Customer
Support may be able to suggest a workaround to avoid this.
Upgrading to the newest version of the compiler may fix this problem.
Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C Compiler". See the link titled
"Submitting an issue". Include this ENTIRE error message and a
copy of the .pp file created when option --preproc_with_comment
(-ppc) is used.
How to fix that problem?Thanks in advance!