Part Number: TMS320F28379D
Tool/software: Code Composer Studio
Hey,
while I'm doing my frist steps in C2000 software development, I found that the compiler adds some NOPs into the compiled code. The optimization is set to -O3, and I use CCSv6.2.
Example:
I made this C-Code for a timing test:
GpioDataRegs.GPATOGGLE.all = 0x80000000;
f_reg_result = AdcaResultRegs.ADCRESULT0;
f_reg_result += AdcaResultRegs.ADCRESULT1;
f_reg_result += AdcaResultRegs.ADCRESULT2;
f_reg_result += AdcaResultRegs.ADCRESULT3;
f_reg_result += AdcaResultRegs.ADCRESULT4;
f_reg_result += AdcaResultRegs.ADCRESULT5;
f_reg_result += AdcaResultRegs.ADCRESULT6;
f_reg_result += AdcaResultRegs.ADCRESULT7;
v_result = f_reg_result / 8;
GpioDataRegs.GPATOGGLE.all = 0x80000000;
The assembly result is this:
174 GpioDataRegs.GPATOGGLE.all = 0x80000000;
082c2f: 1E06 MOVL @0x6, ACC
082c30: 761F002C MOVW DP, #0x2c
175 f_reg_result = AdcaResultRegs.ADCRESULT0;
082c32: E2C40300 UI16TOF32 R3H, @0x0
176 f_reg_result += AdcaResultRegs.ADCRESULT1;
082c34: E2C40201 UI16TOF32 R2H, @0x1
177 f_reg_result += AdcaResultRegs.ADCRESULT2;
082c36: E2C40002 UI16TOF32 R0H, @0x2
176 f_reg_result += AdcaResultRegs.ADCRESULT1;
082c38: E710009B ADDF32 R3H, R3H, R2H
082c3a: 7700 NOP
177 f_reg_result += AdcaResultRegs.ADCRESULT2;
082c3b: E710001B ADDF32 R3H, R3H, R0H
178 f_reg_result += AdcaResultRegs.ADCRESULT3;
082c3d: E2C40203 UI16TOF32 R2H, @0x3
082c3f: 7700 NOP
082c40: E710009B ADDF32 R3H, R3H, R2H
179 f_reg_result += AdcaResultRegs.ADCRESULT4;
082c42: E2C40104 UI16TOF32 R1H, @0x4
082c44: 7700 NOP
082c45: E710005B ADDF32 R3H, R3H, R1H
180 f_reg_result += AdcaResultRegs.ADCRESULT5;
082c47: E2C40005 UI16TOF32 R0H, @0x5
082c49: 7700 NOP
082c4a: E710001B ADDF32 R3H, R3H, R0H
181 f_reg_result += AdcaResultRegs.ADCRESULT6;
082c4c: E2C40106 UI16TOF32 R1H, @0x6
082c4e: 7700 NOP
082c4f: E710005B ADDF32 R3H, R3H, R1H
182 f_reg_result += AdcaResultRegs.ADCRESULT7;
082c51: E2C40007 UI16TOF32 R0H, @0x7
082c53: 7700 NOP
082c54: E710001B ADDF32 R3H, R3H, R0H
082c56: 7700 NOP
183 v_result = f_reg_result / 8;
082c57: E84F8018 MPYF32 R0H, #0x3e00, R3H
082c59: 761F02A0 MOVW DP, #0x2a0
082c5b: E2030000 MOV32 @0x0, R0H
082c5d: 761F01FC MOVW DP, #0x1fc
184 GpioDataRegs.GPATOGGLE.all = 0x80000000;
082c5f: 1E06 MOVL @0x6, ACC
What is the reason for this NOPs?
Best regards,
Thomas.