This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Floats not displaying properly in watch window

I have some TI code that is using IQ Math.

I have compiled the code with MATH_TYPE = FLOAT_MATH

I have the compiler switch set to --float-support=fpu32

In the debugger watch window, the IQ numbers display as long type. I can change the format to "float", but the type is still long. When I view the "IQ" variables (which are really float types) in memory, the display properly when formatted as floats. However the watch window cannot display them properly.

I am using CCSV4 (latest version as of today 2010-Sept-2) and running on the C2000 F28335

How do I get the debugger watch window to understand that these floats are really floats?

 

Thanks