Other Parts Discussed in Thread: IWR1443, UNIFLASH
I have an IWR1443 application that writes calibration data to flash. I need to be able to reflash the BSS and MSS images without Uniflash erasing the entire flash (and my cal data). Or alternately, I could achieve the same thing if I could specify a binary file to be written to an offset of flash while the BSS and MSS images are being written. Is this possible?
thanks, dave
BTW - the Uniflash user guide says to post an issue here, but if you enter a valid "Part number" or you enter Uniflash for the Part number, then you can't select Code Composer Forum.