This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: More 'help description' would be useful to clearly explain what are the best practices for workspace and project cloning, copying and moving

Other Parts Discussed in Thread: CCSTUDIO

Tool/software: Code Composer Studio

The following is just my opinion.

Since I see the same type of questions popping up for years and years, related to ever progressing revisions of the CCStudio I can conclude that there is a clear need for the concise document that gives a list of instructions how to clone CCSStudio Eclipse workspace or CCStudio Eclipse project for:

- one user

- different users on the same windows machine including intricacies related to the Windows OSs

- different developer on a different machine

There seems to be too much confusion about how to handle projects within the workspace, and the solution is typically reinstallation of the workspace, or project, or the whole CCStudio, which is a workaround/

Also, a clear description of the workspace/project/folders/source code relations, and even more important, limitations, should be easily found using the help system within the CCStudio itself.

For example, the fact that the workspace folder is not supposed to overlap with the project folder is neither obvious nor intuitive, and there are scores of developers encountering the same problem over and over again.

A little bit more of explanation would go a long way in even more enjoyment in developing on the otherwise great tool: CCStudio.