Part Number: UCD3138
Tool/software: Code Composer Studio
I tried to build the Firmware for the Evalation Board UCD3138EVM-026 with the Code Composer Studio version 6.1.3. I used the compiler version TI v5.2.5, but it doesn't works.
I get several error Messages:
"Driver/Pmbus/pmbus_command_indexes.asm" "Driver/Pmbus/pmbus_common.asm" "Driver/Pmbus/pmbus_driver.asm"
makefile:185: recipe for target 'clean' failed
Das System kann den angegebenen Pfad nicht finden.
gmake: [clean] Error 3 (ignored)
'Finished clean'
undefined first referenced
symbol in file
--------- ----------------
clear_program_flash_start ./software_interrupt.obj
zero_out_integrity_word_start ./software_interrupt.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "PWR026_PFC_UCD3138.out" not
built
I used the following Settings for the compiler
What could be the cause for this error Messages?