Part Number: TMS320F28069F
Tool/software: Code Composer Studio
I have custom hardware built around the TMS320F28069F and I have not been able to successfully debug/flash it. I am using CCS 7.3.0.00019 with the XDS100v3 debugger. Below are the debugger settings and the schematic involving the JTAG connection. I keep getting short circuit errors ranging from NEAR to FAR or 'distance cannot be measured'.
What conditions can throw this error?
Debugger Test Results
[Result] -----[Print the board config pathname(s)]------------------------------------ C:\Users\Aaron\AppData\Local\TEXASI~1\CCS\ TI\2\0\BrdDat\testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 100- or 510-class product. This utility will load the adapter 'jioserdesusbv3.dll'. The library build date was 'Jul 21 2017'. The library build time was '19:36:41'. The library package version is '7.0.48.0'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. The controller has a version number of '4' (0x00000004). The controller has an insertion length of '0' (0x00000000). This utility will attempt to reset the controller. This utility has successfully reset the controller. -----[Print the reset-command hardware log-file]----------------------------- The scan-path will be reset by toggling the JTAG TRST signal. The controller is the FTDI FT2232 with USB interface. The link from controller to target is direct (without cable). The software is configured for FTDI FT2232 features. The controller cannot monitor the value on the EMU[0] pin. The controller cannot monitor the value on the EMU[1] pin. The controller cannot control the timing on output pins. The controller cannot control the timing on input pins. The scan-path link-delay has been set to exactly '0' (0x0000). An error occurred while hard opening the controller. -----[An error has occurred and this utility has aborted]-------------------- This error is generated by TI's USCIF driver or utilities. The value is '-501' (0xfffffe0b). The title is 'SC_ERR_TEST_MEASURE'. The explanation is: The built-in scan-path length measurement failed. The built-in scan-path reliability tests cannot be performed without knowledge of the scan-path length. Try specifying the scan-path lengths in the command-line options or board configuration file of this utility or debugger. [End: Texas Instruments XDS100v3 USB Debug Probe_0]
Debugger Setup
JTAG Connection Circuit
All help is appreciated!