This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CCSTUDIO: BUGS in CCS 7.2

Part Number: CCSTUDIO

Tool/software: Code Composer Studio

CCS 7.2 forgets settings when you change them. Often.

It appears you can select a project, right click select Properties, add or remove something in a compiler or linker setting, predefined symbol, include path, etc...  And it doesn't save them.  Until you try it a second, or sometimes a third time.

Also, if you have a build configuration using as GNU compiler, select an include path, then change to a build configuration that uses a TI compiler, it crashes.