This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CCSTUDIO: After simply RENAMING a project... Device is held in reset.

Part Number: CCSTUDIO

Tool/software: Code Composer Studio

I took a simple little "blink the LED" demo project, and renamed it.  Opps. It WAS working fine.  Now, no matter what I do, when I try to connect to the XDS100V2 debug probe, it refuses and tells me the device is held in reset.  BUT IT'S NOT.

Error connecting to the target:
(Error -1266 @ 0x0)
Device is held in reset. Take the device out of reset, and retry the operation.
(Emulation package 7.0.48.0)

And this:

M3_wakeupSS: Error connecting to the target: (Error -1266 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 7.0.48.0) 

And I'm not even using the M3.  This is supposed to be an A8.

I have tried rebooting everything I can thing of, except my kitchen sink.  Nothing solves it.

What is the "secret magic" that is now needed to fix this issue?  Because my searches yielded a few results, none of which work.

The connector is working. Everything was working. It worked before I renamed the project.  That is ALL THAT I DID.

I have deleted and recreated the CCXML file several times.  I have tried changing and changing back the project settings.  Nothing works.  My "Test" output is pasted below.

(When with this environment be ready for real use???)

[Start: Texas Instruments XDS100v2 USB Debug Probe]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\scott\AppData\Local\TEXASI~1\CCS\
    ti\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Jul 21 2017'.
The library build time was '19:36:41'.
The library package version is '7.0.48.0'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '4' (0x00000004).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the FTDI FT2232 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for FTDI FT2232 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).

-----[The log-file for the JTAG TCLK output generated from the PLL]----------

There is no hardware for programming the JTAG TCLK frequency.

-----[Measure the source and frequency of the final JTAG TCLKR input]--------

There is no hardware for measuring the JTAG TCLK frequency.

-----[Perform the standard path-length test on the JTAG IR and DR]-----------

This path-length test uses blocks of 64 32-bit words.

The test for the JTAG IR instruction path-length succeeded.
The JTAG IR instruction path-length is 6 bits.

The test for the JTAG DR bypass path-length succeeded.
The JTAG DR bypass path-length is 1 bits.

-----[Perform the Integrity scan-test on the JTAG IR]------------------------

This test will use blocks of 64 32-bit words.
This test will be applied just once.

Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.

The JTAG IR Integrity scan-test has succeeded.

-----[Perform the Integrity scan-test on the JTAG DR]------------------------

This test will use blocks of 64 32-bit words.
This test will be applied just once.

Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.

The JTAG DR Integrity scan-test has succeeded.

[End: Texas Instruments XDS100v2 USB Debug Probe]

  • Well, I managed to fix it. So, for posterity sake, for anyone else who runs into the annoying defect...

    First, just do a "Clean"
    Next, outside of CCS, go inside the project folder:
    Clean out everything in debug, manually. "Clean" doesn't erase everything. Even delete the "Debug" folder itself.
    Delete the .launches folder, including everything in it.
    Delete the *.ccxml file.

    Try to debug it, and see the that is complains (mine is asking for a TM4C1294... ccxml file... I have no idea why it thinks I'm using a TIVA device, when I'm using a BBB.)
    Use the FIle | New menu to create a new Target Configuration File.
    Open it, and verify that it has pre-populated the device you are debugging (BeagleBone Black in my case). If not, select it. Probably no need to press the "test" button, but it couldn't hurt.

    Then try launching with the debug button. for my BBB I was presented with a choice of A8 or M4 (which core I want to load, I assume). I deselected the others, and only loaded the A8 core.
    It worked.
  • The M3 message would be coming from one of the subsystems on the AM335x. There are a few subsystems on the device that have Cortex M cores in them.

    In this case it is the wakeup subsystem "M3_wakeupSS". As far as why CCS asked about the tiva ccxml my thought there is that the tiva one was setup as the default so when you deleted the one associated with your project it then tries to use that one.

    Good to hear that you got things working. Deleting the Launch is something that can help with odd errors like this.

    Regards,
    John