Part Number: TMS320F28379D
Other Parts Discussed in Thread: CONTROLSUITE,
Tool/software: Code Composer Studio
Hi,
I am working on TMS dual core controller. I am facing issues while burning code in 2nd core. For reference i am using Controlsuit dual core blinky example code for both the core. I am able to burn code in 1st core without any difficulty and the code is also running fine, but with 2nd core i am getting following note on consol with failure-
Memory Map Initialization Complete
C28xx_CPU2: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed.
C28xx_CPU2: Error occurred during flash operation: No core matches the pattern 'CPU1'
C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
C28xx_CPU2: Error occurred during flash operation: Timed out waiting for target to halt while executing wr_pll.alg
C28xx_CPU2: Error writing the PLL values (Flash algorithm timed out). Operation cancelled.
C28xx_CPU2: Error occurred during flash operation: No core matches the pattern 'CPU1'
C28xx_CPU2: File Loader: Memory write failed: Unknown error
C28xx_CPU2: GEL: File: D:\PROJECTS\blinky_dc_cpu02\CPU2_FLASH\blinky_dc_cpu02.out: Load failed.
C28xx_CPU2: Error occurred during flash operation: No core matches the pattern 'CPU1'
C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
Please help me with this.
Regards,
Shahina.