This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Transporting a copy of a CCSv4 Project folder

Guru* 84110 points

When I post an example project as a zip file, what can I do to make it as easy as possible for someone else to use that project folder on their CCSv4 installation?

I have tried zipping up the whole project folder, deleting the old project+files from my workspace, then unzipping the same contents back. But the project does not show up in my workspace's C/C++ Projects list, even after closing and re-opening CCS.

The only method I have found to work is:

  1. In Windows Explorer, delete all files from the project MyProj except the source files (I only have three source files, .c, .asm, .tcf)
  2. Zip that project folder to MyProj.zip
  3. In CCS, delete the project MyProj - now the workspace is like another user's would be
  4. Unzip the source files into a folder named MyProj under the workspace
  5. In CCS, create a new project named MyProj and make it be an empty DSP/BIOS project
  6. Now the project exists and the source files are still there

This allows me to port the source files, but I would like to avoid the user having to do the multi-step steps 5 and 6.

Any suggestions on an easy way to zip up a folder and transfer it to another user?

Regards,
RandyP