This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6713B: #35#error "must define RT"

Part Number: TMS320C6713B

Tool/software: Code Composer Studio

Hey Everyone!

I am Akshay. I am working on DSK6713 DSP developer kit. I have created a model in Simulink and was able to successfully generate a ".out" file. Now, I have created a workspace and tried to copy all the files that are necessary to load a program into the board. When I try to build I see a couple of errors. 

I also developed another model. I try to do the same thing as mentioned above it can't generate a model. But, when I somehow load the .out file it works just fine. I would want to know the reason behind why it is not able to build a .out file. 

Also, I'd want to know if we can load a file without building the model. If yes, how?

Thank you.