This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Uniflash should retain folder info for each Meta image.

Other Parts Discussed in Thread: UNIFLASH

When you click a Meta image box or the green Browse button, the folder shown is the last folder accessed by Uniflash.  This is rather inconvenient since it creates situations where you don't know where the file(s) are being loaded from.  So you have to browse to them again to make sure you are loading the right files.  The Load Session browser should also retain it's own last-used folder info.

Thanks, dave

  • I think what would be most useful would be if you put your mouse over the file name if it would then show you the full path of the file.  I could also see clicking the name of image file bringing up the browse dialog at the location of that file since you are in the context of that file.  The Add image button and the Load session button should likely stay using the last used location.  If we switch them to be independent we will definitely have bug reports about how UniFlash is forgetting the location.

    I have filed UNIFLASH-934 to track this

    Regards,

    John