Tool/software: TI C/C++ Compiler
My target is using TI-RTOS... and is in the CC26XX family.
Where can I find out more about these variables:
* xdcRomExternFuncPtr
* xdcRomStatePtr
* xdcRomConstPtr
I think these have something to do with the RTOS_ROM region? Or something like that?
The generated linker script is placing these at address 0x200001000, 1004, and 108
Questions:
What are they used for? Are these pointing at RAM somewhere?
Why there? (ie: +100 into the RAM?) Why not at +0
My concern is this: It appears there are some "pre-allocated" memory locations that I am not aware of in this family
where can I find documentation about the memory map - the CHIP trm is not sufficent, what I think I need is more info about the RTOS, DRIVERLIB, and what it expects in RAM layout.