This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320C6674: Priority of section specifiers in linker command files

Part Number: TMS320C6674


Tool/software: TI C/C++ Compiler

Hello,

The other day, I ran into some unexpected behavior from the 8.2.2 linker, and I have attached a simple CCS project to demonstrate it. I was under the impression (perhaps incorrectly) that "more specific" input section specifiers take priority over "less specific" input section specifiers in a linker command file. For example, in the attached project, I have contrived a linker command file that allocates hello.obj (.const) to GROUP1 and hello.obj (.const:.string) to GROUP2:

      ...

18    GROUP1 > EXAMPLE_MEMORY
19    {
20        hello.obj (.const)
21        hello.obj (.far)
22    }
23
24    GROUP2 > EXAMPLE_MEMORY
25    {
26        hello.obj (.const:.string)
27    }

      ...

When I compile and link, I find that the section specifier on line 26 overrides the one on line 20, and therefore the constant string is allocated to GROUP2. This is what I expected to happen. However, if you change the linker command file as follows and rebuild:

      ...

18    GROUP1 > EXAMPLE_MEMORY
19    {
20        hello.obj (.const, .far)
21    }
22
23    GROUP2 > EXAMPLE_MEMORY
24    {
25        hello.obj (.const:.string)
26    }

      ...

...you will then find that the section specifier on line 20 overrides the one on line 25, and therefore the constant string is allocated to GROUP1. I was expecting these two linker command files to behave identically. I'm hoping that someone can explain why these linker command files behave differently; I haven't been able to find anything on my own.

Thanks in advance,
Dave