This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv4 Time Graphs - Questions

Hi

These questions pertain to CCSv4.1.3 graphs selected by doing Tools->Graph->Single Time

1) Is there a way to make the x-axis refresh start at zero instead of continuing from zero each time the graph is refreshed? It would be really handy for viewing arrays to NOT have the x-axis roll its values and restart at zero.

2) Why does the "reset the graph" button destroy the data. You have to select "show the graph properties" and select OK to get the graph data displayed again.

3) When I select "Toggle measurement marker mode", the cute little bubbles follow my cursor as I move along the x-axis. But if I move the cursor to the point where one of the bubbles exit the left side of the graph, the bubbles are gone and can't get them back. This means you can't use the marker on the left most point. Bug perhaps?

4) Is there a way to delete say the X2 marker without having to start over again?

Cheers

 

  • Hi Eddie,

    Eddie said:
    1) Is there a way to make the x-axis refresh start at zero instead of continuing from zero each time the graph is refreshed? It would be really handy for viewing arrays to NOT have the x-axis roll its values and restart at zero.

    This is a known issue and there are plans to address this

    Eddie said:
    2) Why does the "reset the graph" button destroy the data. You have to select "show the graph properties" and select OK to get the graph data displayed again.

    You clear the display, but the data is still there. If you hit the refresh button, the graph will update.

    Eddie said:
    3) When I select "Toggle measurement marker mode", the cute little bubbles follow my cursor as I move along the x-axis. But if I move the cursor to the point where one of the bubbles exit the left side of the graph, the bubbles are gone and can't get them back. This means you can't use the marker on the left most point. Bug perhaps?

    Yes I see this. It gets cleared somehow. I'll take a closer look at that

    Eddie said:
    4) Is there a way to delete say the X2 marker without having to start over again?

    double-click on the X2 marker. That will clear it

    Thanks

    ki

  • #3 was filed as SDSCM00037910

  • Also like to add another request.

    It would be nice of the x axis reset to zero when you reloaded the code.

    Cheers

  • Thanks gals/guys

    Looks like its fixed in 4.2.4.

    Cheers