Part Number: MSP430FR5739
Tool/software: Code Composer Studio
Hello,
I'm new in MSP430 programming area. In my code I'm trying to work with IO registers as a bit field variables, but
it seems like CCS does not recognize it. My code has following definitions:
#include <msp430.h>
#define _MSP430FR5739_
#define LED1 P1OUT_bit.P1OUT_0
.......
The CCS compiler prints out the following message:
Error: #20 identifier "P1OUT_bit.P1OUT_0" is undefined.
It looks like there is still missing a header file that include definitions for all registers for specific devices.
I'll be thankfull for help with this issue.
Sincerely,
Lavi