This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDXLCDK6748: No rule to make Target

Part Number: TMDXLCDK6748
Other Parts Discussed in Thread: SYSBIOS

Tool/software: Code Composer Studio

Hello,

    I am trying to run the C6000 lab speaking about audio application but i am have this Console message:


**** Build of configuration Debug for project audio_C6000_OPT ****

"C:\\ti\\ccsv7\\utils\\bin\\gmake" -k all
gmake[1]: Entering directory 'C:/TI-RTOS/TI_RTOS_labs_sols_rev4.00/C6000/Labs/Lab_13/LAB_13_C6000_STARTER_audio_OPT/audio_C6000_OPT/Debug'
'Building file: ../opt.cfg'
'Invoking: XDCtools'
"C:/ti/xdctools_3_25_03_72/xs" --xdcpath="C:/ti/bios_6_50_01_12/packages;C:/ti/ccsv7/ccs_base;C:/ti/uia_2_00_06_52/packages;C:/TI_RTOS/C6000/Labs/SYSBIOS_Platforms;" xdc.tools.configuro -o configPkg -t ti.targets.C674 -p evmc6748_TTO -r release -c "C:/Program Files (x86)/Texas Instruments/C6000 Code Generation Tools 7.4.5" --compileOptions "-g --optimize_with_debug" "../opt.cfg"
subdir_rules.mk:75: recipe for target 'build-576447905-inproc' failed
js: "C:/ti/xdctools_3_25_03_72/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: Error: Can't find platform package evmc6748_TTO
gmake[1]: *** [build-576447905-inproc] Error 1
gmake[1]: Leaving directory 'C:/TI-RTOS/TI_RTOS_labs_sols_rev4.00/C6000/Labs/Lab_13/LAB_13_C6000_STARTER_audio_OPT/audio_C6000_OPT/Debug'
gmake: *** No rule to make target 'build-576447905', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-576447905', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-576447905', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-576447905', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-576447905', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-576447905', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-576447905', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-576447905', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-576447905', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'C:/ti/ccsv7/eclipse/LOGICPD_BSL_INSTALL/DSP BSL/lib/evmomapl138_bsl.lib', needed by 'audio_C6000_OPT.out'.
gmake: Target 'all' not remade because of errors.

**** Build Finished ****

 

I am using CCS7 and Compiler v7.4.5. I have read about the sh.exe and the WinAVR files and i deleted them. But the errors are still the same.

Can anyone help please?

Regards

Rabah

  • Problem Errors:

    gmake: *** No rule to make target 'build-576447905', needed by 'configPkg/compiler.opt'. audio_C6000_OPT Unknown C/C++ Problem
    gmake: *** No rule to make target 'C:/ti/ccsv7/eclipse/LOGICPD_BSL_INSTALL/DSP BSL/lib/evmomapl138_bsl.lib', needed by 'audio_C6000_OPT.out'. audio_C6000_OPT Unknown C/C++ Problem
    gmake: Target 'all' not remade because of errors. audio_C6000_OPT C/C++ Problem
    gmake[1]: *** [build-576447905-inproc] Error 1 audio_C6000_OPT C/C++ Problem

    Warnings:

    Build-variable 'LOGICPD_BSL_INSTALL' cannot be resolved. This project may not build as expected. audio_C6000_OPT properties Problems
    Invalid project path: Include path not found (\DSP BSL\inc). audio_C6000_OPT pathentry Path Entry Problem
    Invalid project path: Include path not found (C:\TI_RTOS\C6000\Labs\SYSBIOS_Platforms). audio_C6000_OPT pathentry Path Entry Problem
    Product 'SYS/BIOS' v6.35.4.50 is not currently installed. A compatible version 6.50.1.12 will be used during build. audio_C6000_OPT audio_C6000_OPT Problems
    Product 'System Analyzer (UIA Target)' v1.3.1.08 is not currently installed. A compatible version 2.0.6.52 will be used during build. audio_C6000_OPT audio_C6000_OPT Problems
    This project contains 1 unresolved buildable linked resource(s). The project may not build as expected. audio_C6000_OPT project Problems
    XDCpath repository 'C:/TI_RTOS/C6000/Labs/SYSBIOS_Platforms' cannot be found! Visit project's 'Properties > General > RTSC' tab to adjust the XDCpath. audio_C6000_OPT audio_C6000_OPT Problems
  • My errors have reduced into 3 only:
    Description Resource Path Location Type
    gmake: *** No rule to make target 'build-576447905', needed by 'configPkg/compiler.opt'. audio_C6000_OPT Unknown C/C++ Problem
    gmake: Target 'all' not remade because of errors. audio_C6000_OPT C/C++ Problem
    xdc.tools.configuro: Error: Can't find platform package evmc6748_TTO .xdchelp /audio_C6000_OPT line 51 C/C++ Problem

    I cant resolve these errors. I have tried enter the path for the evmc6748_TTO platform but it is still showing the error.


    Can anyone please help?

    Rabah
  • Hi Rabah,
    Did you see the below related link?
    e2e.ti.com/.../1688294

    See desouza's posts on that thread.

    Thanks
    ki
  • Hi Ki,

       Regarding the issues from the post you sent, i have downloaded the workshop file and it contains the logic pd library and the sysbios platform evmc6748_TTO. But i am still having the same error. I am not figuring out how to use the already supplied files to run the projects in the labs. 

    My errors are:

    Description Resource Path Location Type
    unrecognized attribute (@DirectCall) .xdchelp /audio_C6000_OPT line 188 C/C++ Problem
    fatal error #5: could not open source file "C:/Users/matrixpc/AudioLab13/audio_C6000_OPT/Debug/configPkg/package/cfg/opt_p674.h" .xdchelp /audio_C6000_OPT line 39 C/C++ Problem
    gmake: *** [build-576447905] Error 2 audio_C6000_OPT C/C++ Problem
    gmake: Target 'all' not remade because of errors. audio_C6000_OPT C/C++ Problem
    gmake[1]: *** [build-576447905-inproc] Error 1 audio_C6000_OPT C/C++ Problem

    I think i am doing something wrong! But i cant figure out what?

    Regards

    Rabah

  • Rabah - I've brought this thread to the attention of the TI-RTOS experts. Sorry for the delay.

    ki
  • Rabah,
    can you clean and rebuild and post the current complete console output? As far as I can tell you are using XDCtools 3.25 and SYS/BIOS 6.50 and that's an incompatible combination. Which version of SYS/BIOS do you want to use?