Other Parts Discussed in Thread: CCSTUDIO
Hi,
I have a project which has some compilation and linking warnings and I wanted to see if upgrading CGT to latest one would help to make them go away.
After installing v4.3.7 (downloaded from TI CGT site, not from Help - Software Updatdes ), I changed
a. "Build Properties - CCS Build - TI v4.3.7".
b. "Build Properties - C/C++ Build - Macros - C5500_CG_ROOT" to the directory that CGT v4.3.7 locates.
Then I re-built my project and got the following error messages:
Project build options do not match Global configuration settings. Compiler options specify small model, configuration set for large model
I un-installed v4.3.7, re-installed v.4.3.5, changed back those settings in "Build Properties" and re-started CCSv4 (4.1.2.00027), the error messages still remain.
"Runtime Model Options" is set to "large" for memory model in my project, my questions are:
1. How to modify memory model to "large" in "Global configuration settings" ? Is "Compiler options" referring to my project setting ?
2. Are there any additional settings besides "a" and "b" when CGT is upgraded ?
Thanks,
Yuhua