This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Slow clock when emulator is connected

Hi,

 

I have custom board with F28335, XDS510LC USB emulator, CCS3.3. When connected in CCS via the emulator to board, the processors runs slower than it is supposed to. The crystal is 30 MHz, the PLL is set to x5. With emulator connected the processor runs at 30 MHz. It used to work fine until recently.

Regards