Part Number: CODECOMPOSER
Other Parts Discussed in Thread: CC2640
Tool/software: Code Composer Studio
I am running CCS 7.3.0.00019 in a Windows 10 VMware machine. From the Resource Explorer I cannot "Download and Install" the CC2640R2 Launchpad kit SW. The red progress bar comes up at 10% and then disappears with no accompanying message. I have been able to load the SimpleLink CC2640R2 SDK and the SDK BLE Example pack so I think the general setup is OK.