Part Number: TMS320F28335
Tool/software: Code Composer Studio
Hallo,
i use Matlab/Simulink to generate an CCS-Project. To see the CPU-Load while running the Matlab generated code i want to use RTOS-Analyzer.
To configure this and enable the UIA i need an "application’s configuration file (*,cfg)“ in the Projekt. The Matlab generated projekt done't have a file like this.
How can i add such a file to the Matlab generated Projekt (normal CCS- Projekt), to do the Settings for the RTOS-Analyzer ?
If i want to start the Load Analysis ( Tools -> RTOS Analyzer -> Load Analysis) i get the following error.
Is this error related to the non-existing (*,cfg) file and is solved after solving the first question?
If not how I can specify a custom UIA configuration ?
Software Information:
Version: CCS 7.3.0
Matlab2017b
Windows 8
many thanks
Florian