Part Number: TMS320F28377D
Tool/software: Code Composer Studio
Hi
What is the proper procedure for debugging the dual cores of F2837xD from CCS?
For example, I am loading the software on both the cores ,but to run each core successfully. Which core has to be reset and run first, what should be the other core doing in that state? .I know that CPU1 is the master and should give boot command to CPU2, i''ve included this in my software. After loading the software i''ve been following the below steps
1.Resetting both the cores.
2.Running the second core,which waits for the boot command.
3.Going to main() in the first core, and running the first core.
This procedure is not working every time..I am forced to disconnect both the cores,connect again and repeat the above process.This is taking a lot of time..Please suggest the standard procedure, if it is documented,please share.
Regards,
Naveen.