Part Number: CCSTUDIO
Tool/software: Code Composer Studio
I just did a routine update on my CCS 6.1.3.00034.
It has been working fine and stable --- until after the routine update today >> Help >> Check for updates
Compile OK but when I hit 'deBUG' , I get this message....
Debugger initialization error
Error initializing emulator:
Unable to locate entry point for MSP430_EEM_SetClockControl2
And obviously the code doesn't download into the LP. I've been using the 2433LP for a couple of weeks now with no probs at all. Win 10. So, I'm stuck, nothing similar to this on the forum since 3~4 years.
=======
Unfortunately for me, on my 2nd laptop, also Win10, I did the routine update as well. (OK, I shouldn't have...)
Hit debug, and get a similar message...
TI MSP430 USB1/MSP430
Error initializing emulator:
Could not set device Vcc
And as with the other laptop, this CCS installation was working fine / stable for well over a year !
I could really use some help !
Regards.