Part Number: TPS65917EVM
Other Parts Discussed in Thread: USB2ANY, MSP-FET
Tool/software: Code Composer Studio
Hello,
I have a problem, and I almost tried everything, but zero succes.
So, I need to set up the TPS65917EVM's MSP430 to use SPI communication (partner order stuff), and I want to flash the USB2ANY fw for it.
I connected an MSP-FET430UIF external debugger interface to the EVM's JTAG (supply jumper is off), USB is connected either.
The GUI recognizes the board, can be set up.
CSS identify the debugger finely.
BUT, when try to flash (debug) the MSP the next thing happens:
1.Building the code
2.After building is completed it start the debugger, and try to reach the board.
3.The FET's red led start to blink (blinking=comminucation -> in datasheet) like 2-3times
4.The EVM's reset LED lit.
5.Windows device disconnected sound (TUdum) happens.
6.CSS give error: MSP430: Error connecting to the target: Unknown device
7.After cancel the error windows device plugged in sound playing (tuDUM).
And thats it. No flasing, no debugging, board working fine either the SMPS's and the GUI. But can not be flashed.
Any ideas?
I tried to supply from JTAG, from USB, tried to disconnect or connect the regulator's supply, try to use only the JTAG, tried 2 different debuggers (FETs), tried to use different USB ports, tried to reinstall CSS completely, tried to use both debugger and LP5529 debugger version of the build (i know the LP is for lauchpad but who knows), tried to downgrade and upgrade the FW of the FET, etc.
Thanks in advence :)
Have a nice day,
-Szabi